This section describes a procedure to create a program.
Start performing the task after installing CS+.
(1) Generate code :Configure the peripheral functions built in the microcontroller you are going to use. After completing configuration, generate the code. |
(2) Pin Configrator/Pin View : Used pin is checked. |
(3) Coding :Edit the program (Copy and paste the sample program). |
(4) Build :Build the program (If an error occurs, edit the program again). |
(5) Debugging :Debug the program using QB-R5F100LE-TB and E1. |