Starting CS+

3. Plug-in setting

In this tutorial, the Code Generating functions are used.

In the default setting of CS+, the Code Generating functions are not available.

Set the plug-in by following the below procedure.

Select [Plugi-n Setting] from the [Tool] menu.

After configuring the settings as shown in the figure below,

click [OK].

Select [Yes], then CS+ restarts.