E.3.3 Remove an added file from a project
To remove a file(s) that has been added to the debug-dedicated project by using the method above, select the file(s) on the project tree and then select [Remove from Project] from the context menu.
Figure E.12 | [Remove from Project] Item |