This tab shows the detailed information on projects (main project) categorized by the following and the configuration can be changed.
(1) [File]
(2) [License]
(3) [Notes]
Figure A.12 | Property Panel: [Project] Tab |
[Description of each category]
The detailed information on files is displayed.
|
File name
|
Displays the file name of the file to save the information on the main project.
|
|
Default
|
Name of the main project file
|
|
How to change
|
Changes not allowed
|
|
Absolute path
|
Displays the absolute path of the main project file to save the information on them.
|
|
Default
|
Absolute name of main projects
|
|
How to change
|
Changes not allowed
|
The detailed information on a license is displayed and their configuration can be changed.
|
Use standard edition for floating license
|
Select whether to use only a floating license for the standard edition.
|
|
Default
|
Yes
|
|
How to change
|
Select a value from the drop-down list.
|
|
Restriction
|
Yes
|
Uses a floating license for the standard edition.
|
|
No
|
Uses a floating license for editions other than the standard edition.
|
|
Standard edition for floating license is currently in use
|
Displays if a floating license for the standard edition is used.
|
|
Default
|
Yes
|
|
How to change
|
Changes not allowed
|
The detailed information on records is displayed and their configuration can be changed.
|
Memo
|
Add memos to main projects.
Memo is added one item in one line.
The added memos are displayed as subproperty.
|
|
Default
|
Memo [Number of items]
|
|
How to change
|
Edit by the Text Edit dialog box which appears when clicking the [...] button.
For the subproperty, you can use a text box directly enter the text.
|
|
Restriction
|
Up to 256 characters
Up to 256 characters are allowed.
|