2.6.4 Classify a file into a category

You can create a category under the File node and classify files by the category. This makes it easier to view files added to the project on the project tree, and makes it easier to manage files according to function.

To create a category node, select either one of the Project node, Subproject node, or File node on the project tree, and then select [Add] >> [Add New File...] from the context menu.

Figure 2.55

[Add New Category] Item (For File Node)

Figure 2.56

Project Tree Panel (After Adding Category Node)

 

Remark 1.

The default category name is "New category".
To change the category name, you can use [Rename] from the context menu of the category node.

Remark 2.

You can also add a category node with the same name as the existing category node.

Remark 3.

Categories can be nested up to 20 levels.

 

You can classify files into the created category node by dragging and dropping the file.