2.4.2  
Add an existing subproject
 
Select the Project node on the project tree and if you select [Add] >> [Add Subproject...] on the context menu, the Add Existing Subproject dialog box will open.
Figure 2.18  | Add Existing Subproject Dialog Box  | 
 
 
On the dialog box, specify the subproject file of the subproject to add and click the [Open] button.