This dialog box is used to select the contents of function information and set it to the area that this dialog box is called from.
The following items are explained here.
On the Property panel, select the following properties, and then click the [...] button. |
From the [Link Options] tab, [Specify contents of function information] in the [Variables/functions information] category |
The list of the contents of function information which can be specified for the area that this dialog box is called from is displayed.
Select the check boxes to set the contents.
For details about each item, see the description of link option "-VFINFO" of "CC-RL Compiler User’s Manual".
In the area that this dialog box is called from, if the contents is already set, the check box for that contents will be selected by default. |