This tab shows the detailed information on each C source file, assembly source file, link directive file, object file, and library file categorized by the following and the configuration can be changed.
(1) [Build]
Figure A.8 | Property Panel: [Build Settings] Tab (When Selecting C Source File) |
Figure A.9 | Property Panel: [Build Settings] Tab (When Selecting Assembly Source File) |
Figure A.10 | Property Panel: [Build Settings] Tab (When Selecting Link Directive File) |
Figure A.11 | Property Panel: [Build Settings] Tab (When Selecting Object File) |
Figure A.12 | Property Panel: [Build Settings] Tab (When Selecting Library File) |
[Description of each category]
The detailed information on the build is displayed and the configuration can be changed.
|
Set as build-target
|
Select whether to run a build of the selected file.
|
|
Default
|
Yes
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes
|
Runs a build of the selected file.
|
|
No
|
Does not run a build of the selected file.
|
|
Set individual compile option
|
Select whether to set the compile option that differs from the project settings to the selected C source file.
This property is displayed only when a C source file is selected on the project tree and [Yes] in the [Set as build-target] property is selected.
|
|
Default
|
No
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes
|
Sets the option that differs from the project settings to the selected C source file.
|
|
No
|
Does not set the option that differs from the project settings to the selected C source file.
|
|
Set individual assemble option
|
Select whether to set the assemble option that differs from the project settings to the selected assembly source file.
This property is displayed only when the assembly source file is selected on the project tree and [Yes] in the [Set as build-target] property tab is selected.
|
|
Default
|
No
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes
|
Sets the option that differs from the project settings to the selected assembly source file.
|
|
No
|
Does not set the option that differs from the project settings to the selected assembly source file.
|
|
File type
|
The type of the selected file is displayed.
|
|
Default
|
C source file (when the C source file is selected)
Assembly source file (when the assembly source file is selected)
Link directive (when the link directive file is selected)
Object file (when the object file is selected)
Library file (when the library file is selected)
|
|
How to change
|
Changes not allowed
|