To set options for the assemble phase, select the Build tool node on the project tree and select the [Assemble Options] tab on the Property panel.
You can set the various assemble options by setting the necessary properties in this tab.
Often used options have been gathered under the [Frequently Used Options(for Assemble)] category on the [Common Options] tab.  |