|
r_iican_callback_master_error
|
Performs processing in response to detection of IICA master communication error.
[Syntax]
#include "r_cg_macrodriver.h"
static void r_iican_callback_master_error ( MD_STATUS flag );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
MD_STATUS flag;
|
Cause of communication error
MD_SPT: Stop condition detected
MD_NACK: Acknowledge not detected
(No slave that matches the address/A slave can receive no more data or does not require the next data)
|
[Return value]
None.