|
r_rspin_receive_interrupt
|
Performs processing in response to the receive buffer full interrupts.
Remark | This API function is called to run interrupt processing for the receive buffer full interrupt. |
[Syntax]
static void r_rspin_receive_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.