-   
 
 exd_tsk
 
-   
 
 Terminate and delete invoking task.
 
 void    exd_tsk (void);
 This service call terminates the invoking task normally and deletes the task.
 
 The processing performed at task termination is shown in 
Table 19-4.
 
 The CPU locked state and dispatching disabled state is cancelled.
 
 This service call does not return. In the following cases, this service call causes 
SYSTEM DOWN. 
 
 -	 This service call was issued from non-task.
 
 -	 This service call was issued in the status PSW.IPL > kernel interrupt mask level
 
 Note	 This service call does not have the function to automatically free the resources except the mutex hitherto occupied by the task (e.g., semaphores and memory blocks). Make sure the task frees these resources before it terminates