-   
 
 ref_dtq
 iref_dtq
 
-   
 
 Reference data queue state.
 
 ER      ref_dtq (ID dtqid, T_RDTQ *pk_rdtq);
 ER      iref_dtq (ID dtqid, T_RDTQ *pk_rdtq);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      dtqid;
 
 | 
 ID number of the data queue.
  
 | 
| 
 | 
 T_RDTQ  *pk_rdtq;
 
 | 
 Pointer to the packet returning the data queue state.
  
 | 
 
 [Data queue state packet: T_RDTQ]
 
 
 typedef struct  t_rdtq {
     ID      stskid;         /*Existence of tasks waiting for data transmission*/
     ID      rtskid;         /*Existence of tasks waiting for data reception*/
     UINT    sdtqcnt;        /*Number of data elements in data queue*/
 } T_RDTQ;
 
 | 
 
 These service calls store the detailed information of the data queue (existence of waiting tasks, number of data elements in the data queue, etc.) specified by parameter 
dtqid into the area specified by parameter 
pk_rdtq.
 
 -	 
stskid
Stores whether a task is queued to the transmission wait queue of the data queue.
 
 Value:	ID number of the task at the head of the transmission wait queue
 
 -	 
rtskid
Stores whether a task is queued to the reception wait queue of the data queue.
 
 Value:	ID number of the task at the head of the reception wait queue
 
 -	 
sdtqcnt
Stores the number of data elements in data queue.
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 Note	 When the iref_dtq is issued from task or the ref_dtq is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
  
 | 
| 
 | 
 | 
 Memory access violation. (only for ref_dtq)
  
 -	 The operand-write access to the area indicated by  pk_rdtq has not been permitted to the invoking task.
  
 | 
| 
 | 
 | 
 -	 The data queue specified by  dtqid does not exist.
  
 |