CHAPTER 9 TIME MANAGEMENT FUNCTIONS
This chapter describes the time management functions performed by the RI850V4.
The RI850V4's time management function provides methods to implement time-related processing (
Timer Operations:
Delayed task wakeup,
Timeout,
Cyclic handlers) by using base clock timer interrupts that occur at constant intervals, as well as a function to manipulate and reference the system time.
The system time is a time used by the RI850V4 for performing time management (unit: millisecond).
9.2.1 Base clock timer interrupt
To realize the time management function, the RI850V4 uses interrupts that occur at constant intervals (base clock timer interrupts).
When a base clock timer interrupt occurs, processing related to the RI850V4 time (system time update, task timeout/delay, cyclic handler activation, etc.) is executed.
The RI850V4 does not initialize hardware to generate base clock timer interrupts, so it must be coded by the user.
The following shows the necessary settings when using the OS timer as the base clock timer.
OS Timer Setting Registers
|
|
OSTMn control register (OSTMnCTL)
|
|
OSTMn compare register (OSTMnCMP)
|
|
|
|
|
Note When passing control to the processing related to the base clock timer interrupt, the RI850V4 enables acceptance of EI level maskable interrupts by manipulating the PM
n bits in the priority mask register (PMR) and the ID bit in the program status word (PSW), and issuing the eiret instruction (clearing the in-service priority register (ISPR)).
Therefore, if an EI level maskable interrupt occurs within the base clock timer interrupt processing, the interrupt is accepted.
Note Use the OS timer in the interval timer mode.
9.2.2 Base clock interval
In the RI850V4, service call parameters for time specification are specified in milliseconds.
If is desirable to set 1 ms for the occurrence interval of base clock timer interrupts, but it may be difficult depending on the target system performance (processing capability, required time resolution, or the like).
The interval between occurrences of base clock timer interrupts can be defined as the
Base clock interval: tim_base in the system configuration file.
By specifying the base clock cycle, processing regards that the time equivalent to the base clock cycle elapses during a base clock timer interrupt.
An integer value larger than 1 can be specified for the base clock cycle. Floating-point values such as 2.5 cannot be specified.
9.3.1 Delayed task wakeup
Delayed wakeup the operation that makes the invoking task transit from the RUNNING state to the WAITING state during the interval until a given length of time has elapsed, and makes that task move from the WAITING state to the READY state once the given length of time has elapsed.
Delayed wakeup is implemented by issuing the following service call from the processing program.
Timeout is the operation that makes the target task move from the RUNNING state to the WAITING state during the interval until a given length of time has elapsed if the required condition issued from a task is not immediately satisfied, and makes that task move from the WAITING state to the READY state regardless of whether the required condition is satisfied once the given length of time has elapsed.
A timeout is implemented by issuing the following service call from the processing program.
The cyclic handler is a routine dedicated to cycle processing that is activated periodically at a constant interval (activation cycle).
The RI850V4 handles the cyclic handler as a "non-task (module independent from tasks)". Therefore, even if a task with the highest priority in the system is being executed, the processing is suspended when a specified activation cycle has come, and the control is passed to the cyclic handler.
The RI850V4 manages the states in which each cyclic handler may enter and cyclic handlers themselves, by using management objects (cyclic handler control blocks) corresponding to cyclic handlers one-to-one.
- Basic form of cyclic handlers
When coding a cyclic handler, use a void function with one VP_INT argument (any function name is fine).
The extended information specified with
Cyclic handler information is set for the
exinf argument.
The following shows the basic form of cyclic handlers in C.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void cychdr (VP_INT exinf)
{
.........
return; /*Terminate cyclic handler*/
}
|
- Coding method
Code cyclic handlers using C or assembly language.
When coding in C, they can be coded in the same manner as void type functions coded.
When coding in assembly language, code them according to the calling rules prescribed in the compiler used.
- Stack switching
The RI850V4 switches to the system stack specified in the Basic information when passing control to a cyclic handler, and switches to the relevant stack when returning control from the cyclic handler to the processing program in which a base clock timer interrupt occurred and caused activation of the cyclic handler. Therefore, coding regarding stack switching is not required in a cyclic handler.
- Service call issue
The RI850V4 handles the cyclic handler as a "non-task".
Service calls that can be issued in cyclic handlers are limited to the service calls that can be issued from non-tasks.
Note 1 If a service call (
isig_sem,
iset_flg, etc.) accompanying dispatch processing (task scheduling processing) is issued in order to quickly complete the processing in the cyclic handler during the interval until the processing in the cyclic handler ends, the RI850V4 executes only processing such as queue manipulation, counter manipulation, etc., and the actual dispatch processing is delayed until a return instruction is issued by the cyclic handler, upon which the actual dispatch processing is performed in batch.
- Acceptance of EI level maskable interrupts
When passing control to a cyclic handler, the RI850V4 enables acceptance of EI level maskable interrupts by manipulating the PM
n bits in the priority mask register (PMR) and the ID bit in the program status word (PSW), and issuing the eiret instruction (clearing the in-service priority register (ISPR)).
Therefore, if an EI level maskable interrupt occurs within a cyclic handler, the interrupt is accepted.
9.3.4 Create cyclic handler
In the RI850V4, the method of creating a cyclic handler is limited to "static creation".
Cyclic handlers therefore cannot be created dynamically using a method such as issuing a service call from a processing program.
Static cyclic handler creation means defining of cyclic handlers using static API "CRE_CYC" in the system configuration file.
The system time can be set by issuing the following service call from the processing program.
-
set_tim,
iset_tim
These service calls change the RI850V4 system time (unit: millisecond) to the time specified by parameter
p_systim.
The following describes an example for coding this service call.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void task (VP_INT exinf)
{
SYSTIM p_systim; /*Declares data structure*/
p_systim.ltime = 3600; /*Initializes data structure*/
p_systim.utime = 0; /*Initializes data structure*/
.........
set_tim (&p_systim); /*Set system time*/
.........
}
|
9.5 Reference System Time
The system time can be referenced by issuing the following service call from the processing program.
-
get_tim,
iget_tim
These service calls store the RI850V4 system time (unit: millisecond) into the area specified by parameter
p_systim.
The following describes an example for coding this service call.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void task (VP_INT exinf)
{
SYSTIM p_systim; /*Declares data structure*/
UW ltime; /*Declares variable*/
UH utime; /*Declares variable*/
.........
get_tim (&p_systim); /*Reference System Time*/
ltime = p_systim.ltime; /*Acquirer system time (lower 32 bits)*/
utime = p_systim.utime; /*Acquirer system time (higher 16 bits)*/
.........
}
|
Note 1 The RI850V4 ignores the numeric values that cannot be expressed as the system time (values overflowed from the 48-bit width).
9.6 Start Cyclic Handler Operation
Moving to the operational state (STA state) is implemented by issuing the following service call from the processing program.
-
sta_cyc,
ista_cyc
This service call moves the cyclic handler specified by parameter
cycid from the non-operational state (STP state) to operational state (STA state).
As a result, the target cyclic handler is handled as an activation target of the RI850V4.
The relative interval from when either of this service call is issued until the first activation request is issued varies depending on whether the TA_PHS attribute is specified for the target cyclic handler during configuration.
- If the TA_PHS attribute is specified
The target cyclic handler activation timing is set based on the activation phases (initial activation phase
cycphs and activation cycle
cyctim) defined during configuration.
If the target cyclic handler has already been started, however, no processing is performed even if this service call is issued, but it is not handled as an error.
The following shows a cyclic handler activation timing image.
Figure 9-1 TA_PHS Attribute: Specified
- If the TA_PHS attribute is not specified
The target cyclic handler activation timing is set based on the activation phase (activation cycle
cyctim) when this service call is issued.
This setting is performed regardless of the operating status of the target cyclic handler.
The following shows a cyclic handler activation timing image.
Figure 9-2 TA_PHS Attribute: Not Specified
The following describes an example for coding this service call.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void task (VP_INT exinf)
|
{
ID cycid = ID_CYC1; /*Declares and initializes variable*/
sta_cyc (cycid); /*Start cyclic handler operation*/
.........
}
|
Note
The extended information specified in the Cyclic handler information is passed to the cyclic handler activated by issuing this service call.
9.7 Stop Cyclic Handler Operation
Moving to the non-operational state (STP state) is implemented by issuing the following service call from the processing program.
-
stp_cyc,
istp_cyc
This service call moves the cyclic handler specified by parameter
cycid from the operational state (STA state) to non-operational state (STP state).
As a result, the target cyclic handler is excluded from activation targets of the RI850V4 until issue of
sta_cyc or
ista_cyc.
The following describes an example for coding this service call.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void task (VP_INT exinf)
{
ID cycid = ID_CYC1; /*Declares and initializes variable*/
.........
stp_cyc (cycid); /*Stop cyclic handler operation*/
.........
}
|
Note This service call does not perform queuing of stop requests. If this service call has already been issued and the target cyclic handler has been moved to the non-operational state (STP state), no processing is performed but it is not handled as an error.
9.8 Reference Cyclic Handler State
A cyclic handler status by issuing the following service call from the processing program.
-
ref_cyc,
iref_cyc
Stores cyclic handler state packet (current state, time left before the next activation, etc.) of the cyclic handler specified by parameter
cycid in the area specified by parameter
pk_rcyc.
The following describes an example for coding this service call.
#include <kernel.h> /*Standard header file definition*/
#include <kernel_id.h> /*System information header file definition*/
void task (VP_INT exinf)
{
ID cycid = ID_CYC1; /*Declares and initializes variable*/
T_RCYC pk_rcyc; /*Declares data structure*/
STAT cycstat; /*Declares variable*/
RELTIM lefttim; /*Declares variable*/
ATR cycatr; /*Declares variable*/
RELTIM cyctim; /*Declares variable*/
RELTIM cycphs; /*Declares variable*/
.........
ref_cyc (cycid, &pk_rcyc); /*Reference cyclic handler state*/
cycstat = pk_rcyc.cycstat; /*Reference current state*/
lefttim = pk_rcyc.lefttim; /*Reference time left before the next */
/*activation*/
cycatr = pk_rcyc.cycatr; /*Reference attribute*/
cyctim = pk_rcyc.cyctim; /*Reference activation cycle*/
cycphs = pk_rcyc.cycphs; /*Reference activation phase*/
.........
}
|