Below are #pragma directives supported as extended language specifications.
Allocates variables to an arbitrary section.
For details about the allocation method, see "4.2.4.1 Allocation of data and program to section".
Assembler directives can be described in a C source program.
For the details of description, see "4.2.4.2 Describing assembler instruction".
A function that is expanded inline can be specified.
For the details of expansion specification, see "4.2.4.3 Inline expansion".
You can specify that a function is not eligible for inline expansion.
See "4.2.4.3 Inline expansion" for details about specifying functions to be ineligible for inline expansion.
Interrupt/Exception handlers are described in C language.
For details, see "(3) Describing interrupt/exception handler".
#pragma interrupt [(]function-name[(interrupt specification [,interrupt specification]...)] [,...] [)]  | 
Interrupts are disabled for the entire function.
For details, see "(2) Disabling interrupts in entire function".
Specifies the packing of a structure type. The packing value, which is an alignment value of the member, is specified as the numeric value. A value of 1, 2, 4 can be specified. When the numeric value is not specified, the setting is the default alignment.
For details, see "4.2.4.8 Structure type packing".
CC-RH can switch the order of a bit field.Specifies the switching the order of a bit field.
For details, see "4.2.4.9 Bit field assignment".
A function to which a core number is to be assigned can be specified.
For details, see "4.2.4.10 Core number specification (for a multi-core device)".
This specifies the alignment value for branch destination addresses.
For details, see "4.2.4.11 Specifying alignment value for branch destination addresses".
This specifies a function for generating a code for detection of stack smashing.
For details, see "4.2.4.12 Detection of stack smashing [Professional Edition only]".
This specifies a function for not generating a code for detection of stack smashing.
For details, see "4.2.4.12 Detection of stack smashing [Professional Edition only]".