4.2.4.4
Controlling interrupt level
The CC-RH can manipulate the interrupts of the RH850 family as follows in a C source.
- | By controlling interrupt level |
- | By enabling or disabling acknowledgment of maskable interrupts (by masking interrupts) |
In other words, the interrupt control register can be manipulated.
(1) | Controlling the interrupt priority level |
For this purpose, the "__ set_il" function is used. Specify this function as follows to manipulate the interrupt priority level.
__set_il_rh(int interrupt-priority-level, void* address of interrupt control register);
|
Integer values 1 to 16 can be specified as the interrupt priority level. With RH850, sixteen steps, from 0 to 15, can be specified as the interrupt priority level. To set the interrupt priority level to "5", therefore, specify the interrupt priority level as "6" by this function.
(2) | Enable or disable acknowledgement of maskable interrupts (interrupt mask) |
Specify the __ set_il function as follows to enable or disable acknowledgment of a maskable interrupt.
__set_il_rh(int enables/disables maskable interrupt, void* address of interrupt control register);
|
Integer values -3 to 0 can be specified to enable or disable the maskable interrupt.
|
|
|
|
0
|
Enables acknowledgement of maskable interrupt (unmasks interrupt).
|
|
-1
|
Disables acknowledgment of maskable interrupt (masks interrupt).
|
|
-2
|
To use direct branching (standard specification) as the interrupt vector method
|
|
-3
|
To use table lookup (extended specification) as the interrupt vector method
|