Returns the size of the term section after linking.
[Function]
Returns the size of the term section after linking.
[Application example]
(1)  | Allocates a 4-byte area, and initializes it with the size of the .text section.  | 
 
 
To use this operator in conjunction with STARTOF:
.DW         STARTOF(.data) + SIZEOF(.data) 
 | 
 
[Caution]
-  | SIZEOF can only be written as an operand of the data definition directive, .dw.  | 
 
-  | This operator can be specified in combination with STARTOF by using the binary operator "+". 
Note, however, that it is not possible on the same line to write multiple instances of STARTOF and SIZEOF or include an expression other than STARTOF or SIZEOF.  |