Returns from FE level exception (Return from Trap or Interrupt)
[Syntax]
[Function]
Returns execution from an FE level exception. The return PC and PSW are loaded from the FEPC and FEPSW registers and set in the PC and PSW, and control is passed.
[Description]
- | The assembler generates one feret machine instruction. |
[Flag]
|
CY
|
Value read from FEPSW is set
|
|
OV
|
Value read from FEPSW is set
|
|
S
|
Value read from FEPSW is set
|
|
Z
|
Value read from FEPSW is set
|
|
SAT
|
Value read from FEPSW is set
|