Hyperbolic cosine
[Classification]
Mathematical library
[Syntax]
#include <mathf.h>
float   coshf(float x);
[Return value]
Returns the hyperbolic cosine of x.
coshf returns HUGE_VAL and sets macro ERANGE to global variable errno if an overflow occurs.
[Description]
This function calculates the hyperbolic cosine of x.  Specify the angle in radian.  The definition expression is as follows.
 
(e x + e -x) / 2
[Example]
| #include    <mathf.h> float func(float x) {        float   ret;         ret = coshf(x);     /*Returns value of hyperbolic cosine of x to ret.*/           :         return(ret); } |