-no_warning_num


This option suppresses outputting warning messages of the specified number.

[Specification format]

-no_warning_num=num[,num]...
-no_warning_num=num1-num2

 

-

Interpretation when omitted

All warning messages are output.

[Detailed description]

-

This option suppresses outputting warning messages of the specified number.

-

Specify the error numbers as num, num1, and num2.
If the error number that does not exist, it will be ignored.

-

An error will occur if num, num1, or num2 is omitted.

-

If num1-num2 is specified, it is assumed that error numbers within the range have been specified.

-

The error number specified by this option is the rightmost 5 digits of the 7-digit number following the "W".

-

This option can only control output for warning messages with message numbers (here written with the component number) in the range from 0510000 to 0529999 and from 0550000 to 0559999.

[Example of use]

-

To suppress outputting warning message "W0511146" and "W0511147", describe as:

>ccrl -no_warning_num=11146,11147 -cpu=S2 -dev=dr5f100pj.dvf main.c