4.1.5
Option to process in strict accordance with ANSI standard
If the -ansi option is specified to CC-RL, it will perform processing in strict accordance with the ANSI standard. The differences between when the -ansi option is specified and when not specified are as follows.
Table 4.9 | Processing When -ansi Option Strictly Conforming to Language Specifications is Specified |
|
|
|
|
|
_Bool type
long long type
|
An error occurs.
|
Specification is allowed.
|
|
# line number
|
An error occurs.
|
Treated in same manner as "#line line number".
|
|
Type conversion
|
An error occurs if a function pointer is assigned to a void pointer.
|
Outputs warning message and permits.
|