|
|
|
|
|
Input Options
|
-Input
|
Specifies relocatable files.
|
|
-library
|
Specifies library files.
|
|
-binary
|
Specifies binary files.
|
|
-define
|
Specifies symbol definitions.
|
|
-entry
|
Specifies an entry symbol or entry address.
|
|
-noprelink
|
Selects non-initiation of the prelinker.
|
|
Output Options
|
-form
|
Selects the output file format.
|
|
-debug
|
Debugging information is output to load module files.
|
|
-sdebug
|
Debugging information is output to the .dbg file.
|
|
-nodebug
|
Debugging information is not output.
|
|
-record
|
Selects the record size.
|
|
-end_record [V2.07.00 or later]
|
This option specifies the end record.
|
|
-rom
|
Specifies the section mapping from ROM to RAM.
|
|
-output
|
Specifies the names of files to be output.
|
|
-map
|
Outputs an external symbol-allocation information file.
|
|
-space
|
Data are output to fill unused ranges of memory.
|
|
-message
|
Information-level messages are output.
|
|
-nomessage
|
The output of messages is disabled.
|
|
-msg_unused
|
Messages are output to indicate the presence of externally defined symbols to which there is no reference.
|
|
-byte_count
|
Specifies the number of bytes in a data record.
|
|
-crc
|
Specifies the format for output of the CRC code.
|
|
-padding
|
Padding data are included at the end of each section.
|
|
-vectn
|
Assigns an address to the specified vector number in the variable vector table (for the RX Family and M16C Family).
|
|
-vect
|
Assigns an address to an unused area in the variable vector table (for the RX Family and M16C Family).
|
|
-jump_entries_for_pic
|
Outputs a jump table file (for the PIC function of the RX Family).
|
|
-create_unfilled_area
|
[To be supported by V2.03 and later versions]
Makes spaces created by .OFFSET unfilled.
|
|
List Options
|
-list
|
A linkage list file is output.
|
|
-show
|
Selects the contents to be output in the linkage list file.
|
|
Optimize Options
|
-optimize
|
Selects the items to be optimized at linkage.
|
|
-nooptimize
|
Selects no optimization at linkage.
|
|
-samesize
|
Specifies the minimum size for unification of the same codes.
|
|
-symbol_forbid
|
Specifies symbols for which unreferenced symbol deletion is disabled.
|
|
-samecode_forbid
|
Specifies symbols for which same code unification is disabled.
|
|
-section_forbid
|
Specifies a section where optimization is disabled.
|
|
-absolute_forbid
|
Specifies an address range where optimization is disabled.
|
|
Section Options
|
-start
|
Specifies a section start address.
|
|
-fsymbol
|
Specifies the section where an external defined symbol will be placed in the output file.
|
|
-aligned_section
|
Specifies the section alignment value as 16 bytes.
|
|
Verify Options
|
-cpu
|
Checks addresses for consistency.
|
|
-contiguous_section
|
Specifies sections that will not be divided.
|
|
Other Options
|
-s9
|
Selects the output of an s9 record at the end of the file.
|
|
-stack
|
Selects the output of a stack-usage information file.
|
|
-compress
|
Debugging information are compressed.
|
|
-nocompress
|
Debugging information are not compressed.
|
|
-memory
|
Selects the amount of memory to be used in linkage.
|
|
-rename
|
Specifies symbol names and section names to be modified.
|
|
-delete
|
Specifies symbol names and module names to be deleted.
|
|
-replace
|
Specifies library modules to be replaced.
|
|
-extract
|
Specifies modules to be extracted from library files.
|
|
-strip
|
Debugging information is deleted from absolute files and library files.
|
|
-change_message
|
Specifies changes to the levels of messages (information, warning, and error).
|
|
-hide
|
Name information on local symbols is deleted.
|
|
-total_size
|
The total sizes of sections after linkage are sent to standard output.
|
|
Subcommand File Option
|
-subcommand
|
Specifies a file from which to include command options.
|
|
Options Other Than Above
|
-logo
|
Selects the output of copyright information.
|
|
-nologo
|
Selects the non-output of copyright information.
|
|
-end
|
Selects the execution of option strings specified before END.
|
|
-exit
|
Specifies the end of option specification.
|