Renesas Electronics
Configure the operating environment on the Property panel below when using E20.
Figure 2.36
Example of Property Panel [E20]
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.4.1 [Connect Settings] tab
2.3.4.2 [Debug Tool Settings] tab
2.3.4.3 [Download File Settings] tab
2.3.4.4 [Hook Transaction Settings] tab