2.9.2.1
Change display format of values
The display format of the [value] area can be changed using buttons below on the toolbar.
Notation
|
The following buttons to change the notation of a data value are displayed.
|
|
AutoSelect
|
Displays the value of the selected item (including sub-items) in the default notation (default).
|
Hexadecimal
|
Displays the value of the selected item (including sub-items) in hexadecimal number.
|
Signed Decimal
|
Displays the value of the selected item (including sub-items) in signed decimal number.
|
Unsigned Decimal
|
Displays the value of the selected item (including sub-items) in unsigned decimal number.
|
Octal
|
Displays the value of the selected item (including sub-items) in octal number.
|
Binary
|
Displays the value of the selected item (including sub-items) in binary number.
|
ASCII
|
Displays the character strings of the selected item (including sub-items) in ASCII code.
If the character size is 2 bytes and above, it is displayed with the characters for each 1 byte arranged side-by-side.
|
Float
|
Displays the value of the selected item in Float.
Note that when the value is not 4-byte data, displays it in the default notation.
|
Double
|
Displays the value of the selected item in Double.
Note that when the value is not 8-byte data, displays it in the default notation.
|
|
Adds the value in hexadecimal number enclosing with "()" at the end of the value.
|