A SFR can be searched for.
Specify the SFR name to search with the text box in the search area (case-insensitive). You can either type character strings directly from the key board (up to 512 characters), or select one from the input history via the drop-down list (up to 10 items).
Then, click either one of the following button.
|
Searches up for the SFR name containing the string specified in the text box, and selects the SFR that is found.
|
|
Searches down for the SFR name containing the string specified in the text box, and selects the SFR that is found.
|
Remark 1. | The hidden SFR name being classified with a category can be searched (the category is opened and the SFR is selected). |
Remark 2. | After typing character strings to search, to press the [Enter] key is the same function as clicking the
button, and to press the [Shift] + [Enter] key is the same function as clicking the
button. |