2.5.2.1 Change download conditions for load module files

Follow the steps below in the Download Files dialog box to change the download conditions (object information and symbol information) for load module files.

(1)

Select a load module file

Select a load module file to download in the [Download file list] area.

(2)

Change download conditions

Current download conditions for the selected load module file are displayed in the [Download file property] area.

Change each items displayed in the property.

Download object

Specify whether to download the object information from the specified file.

Default

Yes

Modifying

Select from the drop-down list.

Available values

Yes

Downloads object information.

No

Does not download object information.

Download symbol information

Specify whether to download the symbol information from the specified fileNote 1.

Default

Yes

Modifying

Select from the drop-down list.

Available values

Yes

Downloads symbol information.

No

Does not download symbol information.

Generate the information for

input completion

Select whether to generate the information for the Symbol name completion function when downloadingNote 2.

Default

Yes

Modifying

Select from the drop-down list.

Available values

Yes

Generates the information for the symbol name completion function. (i.e. uses the symbol name completion function.)

No

Does not generate the information for the symbol name completion function. (i.e. does not use the symbol name completion function.)

Note 1.

If the symbol information have not been downloaded, the source level debugging cannot be performed.

Note 2.

When [Yes] is selected, the time taken for downloading and the memory usage on the host machine will increase. We recommend selecting [No] in this item if you do not intend to use the symbol name completion function.

(3)

Click the [OK] button

Enable all the configuration in this dialog box and change the download conditions.