2.8.3  
Stop the program at the arbitrary position (
breakpoint)
 
The program in execution can be stopped at the arbitrary position by setting a breakpoint.  A breakpoint can be set by one-clicking with the mouse.
You need to configure the type of breakpoints to use before setting a breakpoint. 
This section describes the following operations. 
 
2.8.3.1  Set a breakpoint
2.8.3.2  Edit a breakpoint
2.8.3.3  Delete a breakpoint