|
debugger.Register.SetValue
|
This function sets the value of a register, IO register, and SFR.
[Specification format]
debugger.Register.SetValue(regName, value)
|
[Argument(s)]
|
|
|
|
regName
|
Specify the register name to set.
|
|
value
|
Specify the value to set.
|
[Return value]
If the value was set successfully: True
If there was an error when setting the value: False
[Detailed description]
- | This function sets the value specified by value in the register specified by regName. |
[Example of use]
>>>debugger.Register.GetValue("pc")
0x100
>>>debugger.Register.GetValue("A:RB1")
0x20
>>>debugger.Register.SetValue("pc", 0x200)
True
>>>debugger.Register.GetValue("pc")
0x200
>>>
|