2.9	 Start Program Analyzer Tool [RI850V4 V1.xx.xx][RI78V4 V1.xx.xx]
 From [View] menu, select [Realtime OS] >> [Program Analyzer], program analyzer is started.
 
 From [View] menu, select [Realtime OS] >> [Program Analyzer]. The program analyzer is started.
 
 Figure 2-8.    [Program Analyzer] Item
 
 Figure 2-9.    Program Analyzer Window
 
 Remarks 1.	 When program analyzer has started, it isn't possible to start more program analyzer.
 
 2.	 See "RI850V4/RI78V4 Analysis" for details.