Window/Panel/Dialog Box Name
  
 | 
 | 
| 
 | 
 The first window opened when CS+ starts.
  
 | 
 Create Project dialog box
  
 | 
 Creates a new project or subproject.
  
 (See "CS+ Start" for details.)
  
 | 
| 
 | 
 Displays the project elements as a tree.
  
 (See "RI78V4 V2. xx. xx/RI850V4 V2. xx. xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Coding" for details.)
  
 | 
| 
 | 
 Displays details and change the settings of the node selected in the Project Tree panel.
  
 (See "RI78V4 V2. xx. xx/RI850V4 V2. xx. xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User 's Manual: Coding" for details.)
  
 | 
 Realtime OS Resource Information panel
  
 | 
 Displays real-time OS resource information (system information, memory area information, etc.).
  
 (See "RI78V4 V2. xx. xx/RI850V4 V2. xx. xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User 's Manual: Debug" for details.)
  
 | 
 Realtime OS Task Analyzer panel 
  
 [RI78V4 V2 .xx.xx][RI850V4 V2 .xx.xx]
  
 | 
 Displays information required to analyze the processing program (the status of execution transition of programs being processed, usage of real-time OS resources, usage of the CPU, etc.).
  
 (See "RI78V4 V2. xx. xx/RI850V4 V2. xx. xx/RI600V4 Real-Time Operating System User 's Manual: Analysis" for details.)
  
 | 
 Program analyzer window (AZ850V4 window) [RI850V4 V1 .xx.xx]
  
 | 
 Executes basic operation of program analyzer.
  
 (See "RI850V4 Real-Time Operating System User 's Manual: Analysis" for details.)
  
 | 
 Program analyzer window (AZ78K0R window) [RI78V4 V1 .xx.xx]
  
 | 
 Executes basic operation of program analyzer.
  
 (See "RI78V4 Real-Time Operating System User 's Manual: Analysis" for details.)
  
 |