Below chart describes contents of Function List Panel. For the details, refer to help.
"Static" information is described after build. "Dynamic" information is described after connecting the debug tool.
| 
 Description  | 
 Overview  | 
 Static/Dynamic  | 
| 
 Function name  | 
 Function name defined/referenced in C source  | 
 Static  | 
| 
 File name  | 
 File name of C source where the function is defined  | 
 Static  | 
| 
 File Path  | 
 Absolute path of the C source file where the function is defined.  | 
 Static  | 
| 
 Import  | 
 Source of the function information  | 
 Static  | 
| 
 Attribute  | 
 Function's symbol attributes/symbol-modifier attributes  | 
 Static  | 
| 
 Return Type  | 
 Return type of the function  | 
 Static  | 
| 
 Arguments count  | 
 Argument value of the function  | 
 Static  | 
| 
 Arguments  | 
 Argument type/formal argument name of the function  | 
 Static  | 
| 
 Code Size  | 
 Function's code size  | 
 Static  | 
| 
 Stack Size  | 
 Function's stack size  | 
 Static  | 
| 
 Start Address  | 
 Function's start address  | 
 Static  | 
| 
 End Address  | 
 End address of the function  | 
 Static  | 
| 
 Reference Count  | 
 Number of times the function is referenced in the program  | 
 Static  | 
| 
 Execution Count  | 
 Number of times the function was executed  | 
 Dynamic  | 
| 
 Execution Time  | 
 Execution time of the function, Proportion of total, etc..  | 
 Dynamic  | 
| 
 Code Coverage  | 
 Code coverage ratio of the function  | 
 Dynamic  | 
| 
 Total  | 
 Total of above item in the target file  | 
 -  |