This panel allows you to open a tutorial, access (create/open) a project, and load a sample project, with single-click.
The following items are explained here.
Click the 
 button to show a tutorial aimed at improving your understanding of CS+.
Click the 
 button to open the Create Project dialog box, in order to create a new CS+ project file.
Click the 
 button to open the Create Project dialog box, in order to create a new boot loader project and a new application project for multi-core.
This area displays up to four of the most recently used project file names (project names).
This area displays up to four of the project file names (project names) in your favorites.
Click the 
 button to open the Open Project dialog box, in order to open an existing CS+ project file (with ".mtpj" extension).
Click the 
 button to open the Open Project dialog box, in order to open an existing e2 studio project file (with ".rcpc" extension)/CubeSuite project file (with ".cspj" extension)/HEW workspace file (with ".hws" extension)/HEW project file (with ".hwp" extension)/PM+ workspace file (with ".prw" extension)/PM+ project file (with ".prj" extension).
Load a sample project file (with ".mtpj" extension) provided by CS+.
Select the [Microcontroller] tab, then select a sample project from the list.  Next, click the 
 button to open the Browse For Folder dialog box and specify a folder to which to copy the sample project.  After copying the sample to the specified folder, the sample project is loaded.