Below are input conventions for configuring information in the panels and dialog boxes provided by CS+.
The following character sets are allowed for input.
Table D.1  | List of Character Sets  | 
 
| 
 | 
 | 
| 
 
ASCII 
 | 
 
Single-byte numbers, letters, and punctuation 
 | 
| 
 
Shift-JIS 
 | 
 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana 
 | 
| 
 
EUC-JP 
 | 
 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana 
 | 
| 
 
UTF-8 
 | 
 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji (including Chinese), and single-byte Katakana 
 | 
 
Numbers may be input in the following base formats.
Table D.2  | List of Number Bases  | 
 
| 
 | 
 | 
| 
 
Decimal number 
 | 
 
Starts with 1 to 9, followed by a sequence of the digits 0 to 9, and 0 
 | 
| 
 
Hexadecimal number 
 | 
 
Starts with 0x, followed by a sequence of the digits 0 to 9 and the letters a to f 
(As for capital letter/small letter of the alphabet, it is pretermission.) 
 |