[General - External Text Editor] category


Use this category to configure general settings relating to the external text editor.

Figure A.44

Option Dialog Box ([General - External Text Editor] Category)

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Options...].

[Description of each area]

(1)

[Use external text editor]

 

Uses an external text editor as the text editor.

 

Uses the Editor panel as the text editor (default).

(2)

[External text editor path]

Either type in the name of the executable file (including absolute path) for the external text editor directly via the keyboard (up to 259 characters), or click the [Browse...] button, and in the Select External Text Editor dialog box, specify the name of the executable file.

This item is only enabled if the [Use external text editor] check box is selected.

(3)

[Startup options]

Specify the startup options (without the line number) for the external text editor (up to 256 characters).

This item is only enabled if the [Use external text editor] check box is selected.

The following placeholders can be specified by the button.

If you wish to specify more than one option, separate them by spaces.

%FileName%

Passes the name of the file to display to the external text editor.

%FilePath%

Passes the absolute path of the file to display to the external text editor.

%FileRelativePath%

Passes the absolute path of the file from the project folder to display to the external text editor.

%Line%

Passes the caret position (line number) to the external text editor.

(4)

[Startup options (with line number)]

Specify the startup options (with the line number) for the external text editor (up to 256 characters).

This item is only enabled if the [Use external text editor] check box is selected.

The following placeholders can be specified by the button.

If you wish to specify more than one option, separate them by spaces.

%FileName%

Passes the name of the file to display to the external text editor.

%FilePath%

Passes the absolute path of the file to display to the external text editor.

%FileRelativePath%

Passes the absolute path of the file from the project folder to display to the external text editor.

%Line%

Passes the caret position (line number) to the external text editor.

(5)

[Open in internal editor during debug]

This item is only enabled if the [Use external text editor] check box is selected.

 

Suppresses starting an external text editor and opens the file to display in the Editor panel during debugging (default).

 

Opens the file to display in an external text editor.

(6)

Buttons

Initialize Settings

Returns all currently displayed setting to their default values.

[Function buttons]

Button

Function

Initialize All Settings

Restores all settings on this dialog box to their default values.

Note, however, that newly added items in the [General - External Tools] category will not be removed.

OK

Applies all setting and closes this dialog box.

Cancel

Ignores the setting and closes this dialog box.

Apply

Applies all setting (does not close this dialog box).

Help

Displays the help of this dialog box.