Renesas Electronics
To set options for the link phase, select the Build tool node on the project tree and select the [Librarian Options] tab on the Property panel.
You can set the various librarian options by setting the necessary properties in this tab.
Caution
This tab is not displayed for the application project.
Figure 2.64
Property Panel: [Librarian Options] Tab