-A


This option performs conversion with the -za option (which is an ANSI-compliant option of CA78K0) enabled.

[Specification format]

-A

 

-

Interpretation when omitted

Conversion is performed with the -za option disabled.

[Detailed description]

-

When this option is specified, the following words are not regarded as keywords and they will not be converted.

callt, sreg, boolean, bit

-

Specify this option if the -za option is used in the CA78K0 development environment before conversion.

[Example of use]

>CcnvCA78K0  input.c  -o=output.c  -A