r_ostmm_interrupt


Performs processing in response to the OS timer interrupt.

Remark

This API function is called as the interrupt process corresponding to the OS timer interrupt.

[Syntax]

void    r_ostmm_interrupt ( void );

Remark

m is the channel number.

[Argument(s)]

None.

[Return value]

None.