r_cmtw_icmin_interrupt


Performs processing in response to the input capture interrupt.

[Syntax]

static  void    r_cmtw_icmin_interrupt ( void );

Remark

m is the timer general register number, n is the channel number.

[Argument(s)]

None.

[Return value]

None.