Renesas Electronics
R_CRC_Get_Result
Gets the result of operation.
[Syntax]
#include "r_cg_macrodriver"
void R_CRC_Get_Result ( uint8_t * const result );
[Argument(s)]
I/O
Argument
Description
O
uint8_t * const result;
Pointer to the location where the result of operation is stored
[Return value]
None.