r_dmacn_callback_transfer_end


Performs processing in response to the transfer end interrupt.

Remark

This API function is called as thecall r_dmac_dmacni_interrupt back routine.

 

[Syntax]

static  void    r_dmacn_callback_transfer_end ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.