Renesas Electronics
R_DOC_GetResult
Gets the result of operation.
[Syntax]
#include "r_cg_macrodriver"
void R_DOC_GetResult ( uint16_t * const data );
[Argument(s)]
I/O
Argument
Description
O
uint16_t * const data;
Pointer to the location where the result of operation is to be stored
[Return value]
None.