Allows starting the data transfer controller.
Remark | In this API function, starting the data transfer controller is allowed by operating the DTCE bit of the DTC activation enable register n (DTCERn) supporting the transfer data number m.
m is the transfer data number, n is the interrupt vector number.
|
[Syntax]
void R_DTCm_Start ( void );
|
Remark | m is the transfer data number. |
[Argument(s)]
None.
[Return value]
None.