Renesas Electronics
R_LPC_Sleep
Transits the low power consumption mode of the MCU to the sleep mode.
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_LPC_Sleep ( void );
[Argument(s)]
None.
[Return value]
Macro
Description
MD_OK
Normal completion
MD_ERROR1
Exit with error (abend)