r_lvd_lvdn_interrupt


Performs processing in response to the voltage monitoring n interrupt.

Remark

This API function is called to run interrupt processing for the voltage monitoring n interrupt, which is generated when the voltage detection circuit detects the voltage being dropped.

[Syntax]

static  void    r_lvd_lvdn_interrupt ( void );

Remark

n is the circuit number.

[Argument(s)]

None.

[Return value]

None.