R_S12ADn_Set_CompareValue


Sets compare level.

[Syntax]

void    R_S12ADn_Set_CompareValue ( ad_channel_t  reg_value0,  rad_channel_t  reg_value1 );

Remark

n is the unit number.

[Argument(s)]

I/O

Argument

Description

I

ad_chanel_t  reg_value0

Register value set to the compare revel register 0

I

ad_chanel_t  reg_value1

Register value set to the compare revel register 1

[Return value]

None.