2.3 Enter Information

Configure the information necessary to control the peripheral functions (clock generator, port functions, etc.) in the information setting area of the Peripheral Functions panel which is opened as described in "2.2 Open Peripheral Functions Panel”.

Remark

When controlling multiple peripheral functions, repeat the procedures described in "2.2 Open Peripheral Functions Panel" through "2.3 Enter Information".