1.1 Overview

The Code Generator, which is one of the components provided by CS+, enables you to output the source code (device driver programs, C source files and header files) necessary to control the peripheral functions (clock generator, port functions, etc.) provided by the microcontroller by configuring various information using the GUI.

There are 3 types of products depending on the supporting device *1.

*1 Code Generator Plug-in (for V850, 78K0, 78K0R, RL78/G12, G12, G14, G1A, I1A, L12, F12, F13, F14)

Code Generator/Pin View Plug-in (for RX, RL78 not listed in Code Generator Plug-n)

Code Generator Plug-in for RH850 (for RH850)