sns_dsp

Outline

Reference dispatching state.

C format

 BOOL      sns_dsp ( void );


Assembly format

 CALL    !!_sns_dsp


Parameter(s)

None.

Explanation

This service call acquires the system status type when this service call is issued (dispatching disabled state or dispatching enabled state).

When this service call is terminated normally, the acquired system state type (TRUE: dispatching disabled state, FALSE: dispatching enabled state) is returned.

Note The system enters the dispatching disabled state when dis_dsp is issued, and enters the dispatching enabled state when ena_dsp is issued.

Return value

Macro

Value

Description

TRUE

1

Normal completion (dispatching disabled state).

FALSE

0

Normal completion (dispatching enabled state).