|
-lang [V1.07.00 or later]
|
This option specifies the language standard.
[Specification format]
- | Interpretation when omitted |
Compilation is performed according to the C90 standard.
[Detailed description]
- | This option specifies the language standard of the C source file. |
- | If the -lang=c option is specified or this option is omitted, compilation is performed according to the C90 standard. |
- | If the -lang=c99 option is specified, compilation is performed according to the C99 standard. |
- | If a value other than c or c99 is specified, an error will occur. |