This option enables the PIROD facility.
The PIROD facility is disabled.
The PIROD facility makes the section to which constant data, such as const variables or string literal, is allocated position-independent. |
See "4.2.4.1 Allocation of function and data to section" and "8.6 PIC/PID Facility" for details about the PIROD facility.
When this option is specified, the section to which constant data is output is changed from the const attribute section to the pcconst32 attribute section. |
Referencing constant data allocated to the pcconst32 attribute section is always performed in PC-relative mode. This allows the pcconst32 attribute section to be allocated at a desired address after linkage. |